RunSimulationBuilderCollisionCheckOptions Enumeration¶
NXOpen.Tooling.RunSimulationBuilder.CollisionCheckOptions is an alias for NXOpen.Tooling.RunSimulationBuilderCollisionCheckOptions
-
class
NXOpen.Tooling.
RunSimulationBuilderCollisionCheckOptions
¶ Bases:
object
Specifies the collision check method
Enum Members
Enum Member Enum Member Description FacetBodyDistance Measure facet bodies distance to do collision check MeshTriangleIntersection Mesh facet body, check the mesh triangle intersection or not SolidBodyIntersection Get the solid body, use intersection boolean result to do collision check -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-