ReusePositioningObjectBuilderTypes Enumeration¶
NXOpen.Tooling.ReusePositioningObjectBuilder.Types is an alias for NXOpen.Tooling.ReusePositioningObjectBuilderTypes
-
class
NXOpen.Tooling.
ReusePositioningObjectBuilderTypes
¶ Bases:
object
the positioning types
Enum Members
Enum Member Enum Member Description PatternLinear linear type PatternCircular circular type ImportedData imported data type EditSketch edit sketch type EditMode dialog edit mode QuickCsys quick datum csys mode OffsetCsysPattern offset csys pattern mode PlanarPattern planar type NonPlanarPattern non planar type CurvePattern non planar curve type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-