RenameAndExportComponentBuilderDefinitionType Enumeration

NXOpen.Tooling.RenameAndExportComponentBuilder.DefinitionType is an alias for NXOpen.Tooling.RenameAndExportComponentBuilderDefinitionType

class NXOpen.Tooling.RenameAndExportComponentBuilderDefinitionType

Bases: object

definition type

Enum Members

Enum Member Enum Member Description
Directory
RootPart
Selection
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.