QuickQuotationBuilderTypes Enumeration

NXOpen.Tooling.QuickQuotationBuilder.Types is an alias for NXOpen.Tooling.QuickQuotationBuilderTypes

class NXOpen.Tooling.QuickQuotationBuilderTypes

Bases: object

Specify the operation type.

Enum Members

Enum Member Enum Member Description
JobInformation job information type
ProjectDefinition project definition type
ConceptDesign concept design type
Grouping grouping type
Quoting quoting type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.