QuickQuotationBuilderObjectTypes Enumeration

NXOpen.Tooling.QuickQuotationBuilder.ObjectTypes is an alias for NXOpen.Tooling.QuickQuotationBuilderObjectTypes

class NXOpen.Tooling.QuickQuotationBuilderObjectTypes

Bases: object

Specify the concept sheet body type.

Enum Members

Enum Member Enum Member Description
Piercing sheet body type is piercing
Bending sheet body type is piercing
Forming sheet body is forming
Burring sheet body is burring
Cam sheet body is camunits.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.