PunchInsertBuilderNormalClearanceOptionTypeItems Enumeration¶
NXOpen.Tooling.PunchInsertBuilder.NormalClearanceOptionTypeItems is an alias for NXOpen.Tooling.PunchInsertBuilderNormalClearanceOptionTypeItems
-
class
NXOpen.Tooling.
PunchInsertBuilderNormalClearanceOptionTypeItems
¶ Bases:
object
Specifies the design option of piercing insert.
Enum Members
Enum Member Enum Member Description Constant The design option is normal Variable The design option is fineblanking SuperOffset The design option is fineblanking -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-