PrebendBuilderNumberBendsOption Enumeration¶
NXOpen.Tooling.PrebendBuilder.NumberBendsOption is an alias for NXOpen.Tooling.PrebendBuilderNumberBendsOption
-
class
NXOpen.Tooling.
PrebendBuilderNumberBendsOption
¶ Bases:
object
The option of bend number to divide into
Enum Members
Enum Member Enum Member Description Two two prebends Three three prebends Four four prebends Five five prebends Six six prebends -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-