PiercingInsertBuilderTypes Enumeration¶
NXOpen.Tooling.PiercingInsertBuilder.Types is an alias for NXOpen.Tooling.PiercingInsertBuilderTypes
-
class
NXOpen.Tooling.
PiercingInsertBuilderTypes
¶ Bases:
object
Specifies the option of piercing insert type.
Enum Members
Enum Member Enum Member Description DieInsert the die insert type DieCavityAndSlugHole the die cavity and slug hole type PunchInsert the punch insert type Association the association type Delete the delete insert type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-