PiercingInsertBuilderPunchPocketTypeItemsBP Enumeration¶
NXOpen.Tooling.PiercingInsertBuilder.PunchPocketTypeItemsBP is an alias for NXOpen.Tooling.PiercingInsertBuilderPunchPocketTypeItemsBP
-
class
NXOpen.Tooling.
PiercingInsertBuilderPunchPocketTypeItemsBP
¶ Bases:
object
Specifies the punch pocket type in backing plate.
Enum Members
Enum Member Enum Member Description Clearance Punch pocket type in backing plate is clearance Fillet Punch pocket type in backing plate is fillet Circle Punch pocket type in backing plate is circle -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-