PiercingInsertBuilderNormalUdpparentPartType Enumeration¶
NXOpen.Tooling.PiercingInsertBuilder.NormalUdpparentPartType is an alias for NXOpen.Tooling.PiercingInsertBuilderNormalUdpparentPartType
-
class
NXOpen.Tooling.
PiercingInsertBuilderNormalUdpparentPartType
¶ Bases:
object
Specifies the parent part of user defined punch.
Enum Members
Enum Member Enum Member Description PrjDie099 Parent part is die PrjDb000 Parent part is db PrjSub002 Parent part is sub -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-