PiercingInsertBuilderAssociationToolType Enumeration¶
NXOpen.Tooling.PiercingInsertBuilder.AssociationToolType is an alias for NXOpen.Tooling.PiercingInsertBuilderAssociationToolType
-
class
NXOpen.Tooling.
PiercingInsertBuilderAssociationToolType
¶ Bases:
object
Specifies the association tool operation option.
Enum Members
Enum Member Enum Member Description AddIntoList The operation option is add into list RemoveFromList The operation option is remove from list DeleteSelectedInserts The operation option is delete selected inserts -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-