ObjectAttributeManagementBuilderShowType Enumeration

NXOpen.Tooling.ObjectAttributeManagementBuilder.ShowType is an alias for NXOpen.Tooling.ObjectAttributeManagementBuilderShowType

class NXOpen.Tooling.ObjectAttributeManagementBuilderShowType

Bases: object

show attributes of selected objects or show objects according to attribute

Enum Members

Enum Member Enum Member Description
ShowAttributeOfSelectedObject
ShowObjectAccordingToAttribute
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.