ObjectAttributeManagementBuilderFilterType Enumeration

NXOpen.Tooling.ObjectAttributeManagementBuilder.FilterType is an alias for NXOpen.Tooling.ObjectAttributeManagementBuilderFilterType

class NXOpen.Tooling.ObjectAttributeManagementBuilderFilterType

Bases: object

the selection filter type

Enum Members

Enum Member Enum Member Description
Part
Component
SolidBody
Face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.