MoldFillingBuilderMoveOption Enumeration¶
NXOpen.Tooling.MoldFillingBuilder.MoveOption is an alias for NXOpen.Tooling.MoldFillingBuilderMoveOption
-
class
NXOpen.Tooling.
MoldFillingBuilderMoveOption
¶ Bases:
object
The modification options of the selected fill component.
Enum Members
Enum Member Enum Member Description Move Modifying current component CopyInstance Copying instance and Modifying CopyPart Copying new part and Modifying -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-