MoldCsysBuilderWcsposition Enumeration

NXOpen.Tooling.MoldCsysBuilder.Wcsposition is an alias for NXOpen.Tooling.MoldCsysBuilderWcsposition

class NXOpen.Tooling.MoldCsysBuilderWcsposition

Bases: object

Represents the method to computer the WCS positino

Enum Members

Enum Member Enum Member Description
CurrentWcs current wcs position
ProductBodyCenter product body center position
BoundaryFaceCenter boundary face center position
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.