MWMoldedPartValidationBuilderCalculateOption Enumeration¶
NXOpen.Tooling.MWMoldedPartValidationBuilder.CalculateOption is an alias for NXOpen.Tooling.MWMoldedPartValidationBuilderCalculateOption
-
class
NXOpen.Tooling.
MWMoldedPartValidationBuilderCalculateOption
¶ Bases:
object
Calculation options
Enum Members
Enum Member Enum Member Description KeepExisting calculate and keep existing properties on the faces EditRegionsOnly edit properties of region faces only ResetAll calculate and replace all properties for region faces -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-