MWDesignPartingSurfaceBuilderTrimAndExtendFromRegionType Enumeration¶
NXOpen.Tooling.MWDesignPartingSurfaceBuilder.TrimAndExtendFromRegionType is an alias for NXOpen.Tooling.MWDesignPartingSurfaceBuilderTrimAndExtendFromRegionType
-
class
NXOpen.Tooling.
MWDesignPartingSurfaceBuilderTrimAndExtendFromRegionType
¶ Bases:
object
The region type from which to trim and extend when creating parting surface.
Enum Members
Enum Member Enum Member Description Cavity From cavity region Core From core region NotSet New option for guided extension surface only -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-