MWDesignPartingSurfaceBuilderTransitionSurfaceType Enumeration¶
NXOpen.Tooling.MWDesignPartingSurfaceBuilder.TransitionSurfaceType is an alias for NXOpen.Tooling.MWDesignPartingSurfaceBuilderTransitionSurfaceType
-
class
NXOpen.Tooling.
MWDesignPartingSurfaceBuilderTransitionSurfaceType
¶ Bases:
object
The type of transition surface to be created.
Enum Members
Enum Member Enum Member Description Auto Auto transition surface BoundedPlane Bounded transition surface Swept Swept transition surface Bridge Bridge transition surface -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-