MWDesignGuideLinesBuilderDirectionType Enumeration¶
NXOpen.Tooling.MWDesignGuideLinesBuilder.DirectionType is an alias for NXOpen.Tooling.MWDesignGuideLinesBuilderDirectionType
-
class
NXOpen.Tooling.
MWDesignGuideLinesBuilderDirectionType
¶ Bases:
object
The type of direction for the guide line to be created.
Enum Members
Enum Member Enum Member Description Normal Normal Tangential Tangential SnaptoWCSAxis Snap to WCS axis Vector Specify Vector -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-