LsdynaGeometryPreparationBuilderTargetPunch Enumeration¶
NXOpen.Tooling.LsdynaGeometryPreparationBuilder.TargetPunch is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderTargetPunch
-
class
NXOpen.Tooling.
LsdynaGeometryPreparationBuilderTargetPunch
¶ Bases:
object
the enum of target punch type.
Enum Members
Enum Member Enum Member Description Punch For the process, the target of punch is punch. Binder For the process, the target of punch is binder. Die For the process, the target of punch is die. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-