LsdynaGeometryPreparationBuilderProcessType Enumeration¶
NXOpen.Tooling.LsdynaGeometryPreparationBuilder.ProcessType is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderProcessType
-
class
NXOpen.Tooling.
LsdynaGeometryPreparationBuilderProcessType
¶ Bases:
object
the enum of process type.
Enum Members
Enum Member Enum Member Description Gravity Blank has elastic deformation in flexible status. Closing The process of die travels from initial position to binder. Drawing The process of die travels from binder to punch. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-