LsdynaGeometryPreparationBuilderProcessActionDie Enumeration¶
NXOpen.Tooling.LsdynaGeometryPreparationBuilder.ProcessActionDie is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderProcessActionDie
-
class
NXOpen.Tooling.
LsdynaGeometryPreparationBuilderProcessActionDie
¶ Bases:
object
the enum of process action die type.
Enum Members
Enum Member Enum Member Description Stationary The process action for die is stationary. ClosureWith The process action for die is closure with other draw components. FollowWith The process action for die is follow with other draw components. Travel The process action for die is travel to other draw components. UntilHome The process action for die is until home. Force The process action for die is by force. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-