LsdynaGeometryPreparationBuilderDrawType Enumeration¶
NXOpen.Tooling.LsdynaGeometryPreparationBuilder.DrawType is an alias for NXOpen.Tooling.LsdynaGeometryPreparationBuilderDrawType
-
class
NXOpen.Tooling.
LsdynaGeometryPreparationBuilderDrawType
¶ Bases:
object
the enum of draw type.
Enum Members
Enum Member Enum Member Description SingleDraw For draw die, punch and binder are lower than die. DoubleDraw For draw die, punch and binder are higher than die. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-