LayoutRepositionBuilder Class¶
-
class
NXOpen.Tooling.
LayoutRepositionBuilder
¶ Bases:
NXOpen.Builder
Represents a Tooling::LayoutRepositionBuilder builder
To create a new instance of this class, use
NXOpen.Tooling.MWLayoutCollection.CreateLayoutRepositionBuilder()
Default values.
Property Value DimX.Value 0 (millimeters part), 0 (inches part) DimY.Value 0 (millimeters part), 0 (inches part) RepositionType Move RotateAngle.Value 180 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DimX | Returns the distance dimension in X-axis |
DimY | Returns the distance dimension in Y-axis |
PointFrom | Returns or sets the transform start point |
PointTo | Returns or sets the transform end point |
RepositionMethod | Returns or sets the reposition method |
RepositionType | Returns or sets the reposition type |
RotateAngle | Returns the rotate angle |
RotatePoint | Returns or sets the rotate point |
SelectInstance | Returns the select instance |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LayoutRepositionBuilderMethod Enumeration | Represents the type of layout transform. |
LayoutRepositionBuilderType Enumeration | Represents the method of layout transform. |
Property Detail¶
DimX¶
-
LayoutRepositionBuilder.
DimX
¶ Returns the distance dimension in X-axis
-------------------------------------
Getter Method
Signature
DimX
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
DimY¶
-
LayoutRepositionBuilder.
DimY
¶ Returns the distance dimension in Y-axis
-------------------------------------
Getter Method
Signature
DimY
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
PointFrom¶
-
LayoutRepositionBuilder.
PointFrom
¶ Returns or sets the transform start point
-------------------------------------
Getter Method
Signature
PointFrom
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointFrom
Parameters: pointFrom ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
PointTo¶
-
LayoutRepositionBuilder.
PointTo
¶ Returns or sets the transform end point
-------------------------------------
Getter Method
Signature
PointTo
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointTo
Parameters: pointTo ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
RepositionMethod¶
-
LayoutRepositionBuilder.
RepositionMethod
¶ Returns or sets the reposition method
-------------------------------------
Getter Method
Signature
RepositionMethod
Returns: Return type: NXOpen.Tooling.LayoutRepositionBuilderMethod
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RepositionMethod
Parameters: enumRepositionmethod ( NXOpen.Tooling.LayoutRepositionBuilderMethod
) –New in version NX6.0.0.
License requirements: None.
RepositionType¶
-
LayoutRepositionBuilder.
RepositionType
¶ Returns or sets the reposition type
-------------------------------------
Getter Method
Signature
RepositionType
Returns: Return type: NXOpen.Tooling.LayoutRepositionBuilderType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RepositionType
Parameters: enumRepositiontype ( NXOpen.Tooling.LayoutRepositionBuilderType
) –New in version NX6.0.0.
License requirements: None.
RotateAngle¶
-
LayoutRepositionBuilder.
RotateAngle
¶ Returns the rotate angle
-------------------------------------
Getter Method
Signature
RotateAngle
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
RotatePoint¶
-
LayoutRepositionBuilder.
RotatePoint
¶ Returns or sets the rotate point
-------------------------------------
Getter Method
Signature
RotatePoint
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotatePoint
Parameters: rotatePoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: None.
SelectInstance¶
-
LayoutRepositionBuilder.
SelectInstance
¶ Returns the select instance
-------------------------------------
Getter Method
Signature
SelectInstance
Returns: Return type: NXOpen.SelectBodyList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LayoutRepositionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.