LayoutManagementBuilder Class¶
-
class
NXOpen.Tooling.
LayoutManagementBuilder
¶ Bases:
NXOpen.Builder
Layout Management Builder of Engineering Die Wizard
To create a new instance of this class, use
NXOpen.Tooling.LayoutManagementCollection.CreateLayoutManagementBuilder()
Default values.
Property Value RepositionMotion.DeltaEnum ReferenceWcsWorkPart RepositionMotion.DeltaXc.Value 0.0 RepositionMotion.DeltaYc.Value 0.0 RepositionMotion.DeltaZc.Value 0.0 StationDistance 0 StationEnum One StationNameStr station StationNumber 3 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
BodiesReposition | Returns the select bodies to reposition |
RepositionMotion | Returns the reposition motion |
SelectEntityAdd | Returns the select entity to add into the station |
SelectEntityRemove | Returns the select entity to remove from the station |
SpecifyDieTip | Returns or sets the specify die tip to define the forming direction |
StationDistance | Returns or sets the station distance of engineering die |
StationEnum | Returns or sets the station number definition of engineering die |
StationNameStr | Returns or sets the station name definition of engineering die |
StationNumber | Returns or sets the total station number of engineering die layout |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LayoutManagementBuilderStationItems Enumeration | Specifies the station items |
Property Detail¶
BodiesReposition¶
-
LayoutManagementBuilder.
BodiesReposition
¶ Returns the select bodies to reposition
-------------------------------------
Getter Method
Signature
BodiesReposition
Returns: Return type: NXOpen.SelectBodyList
New in version NX8.0.0.
License requirements: None.
RepositionMotion¶
-
LayoutManagementBuilder.
RepositionMotion
¶ Returns the reposition motion
-------------------------------------
Getter Method
Signature
RepositionMotion
Returns: Return type: NXOpen.GeometricUtilities.ModlMotion
New in version NX8.0.0.
License requirements: None.
SelectEntityAdd¶
-
LayoutManagementBuilder.
SelectEntityAdd
¶ Returns the select entity to add into the station
-------------------------------------
Getter Method
Signature
SelectEntityAdd
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
SelectEntityRemove¶
-
LayoutManagementBuilder.
SelectEntityRemove
¶ Returns the select entity to remove from the station
-------------------------------------
Getter Method
Signature
SelectEntityRemove
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.0.0.
License requirements: None.
SpecifyDieTip¶
-
LayoutManagementBuilder.
SpecifyDieTip
¶ Returns or sets the specify die tip to define the forming direction
-------------------------------------
Getter Method
Signature
SpecifyDieTip
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecifyDieTip
Parameters: specifyDieTip ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: None.
StationDistance¶
-
LayoutManagementBuilder.
StationDistance
¶ Returns or sets the station distance of engineering die
-------------------------------------
Getter Method
Signature
StationDistance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StationDistance
Parameters: stationDistance (float) – New in version NX8.0.0.
License requirements: None.
StationEnum¶
-
LayoutManagementBuilder.
StationEnum
¶ Returns or sets the station number definition of engineering die
-------------------------------------
Getter Method
Signature
StationEnum
Returns: Return type: NXOpen.Tooling.LayoutManagementBuilderStationItems
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StationEnum
Parameters: stationEnum ( NXOpen.Tooling.LayoutManagementBuilderStationItems
) –New in version NX8.0.0.
License requirements: None.
StationNameStr¶
-
LayoutManagementBuilder.
StationNameStr
¶ Returns or sets the station name definition of engineering die
-------------------------------------
Getter Method
Signature
StationNameStr
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StationNameStr
Parameters: stationNameStr (str) – New in version NX8.0.0.
License requirements: None.
StationNumber¶
-
LayoutManagementBuilder.
StationNumber
¶ Returns or sets the total station number of engineering die layout
-------------------------------------
Getter Method
Signature
StationNumber
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StationNumber
Parameters: stationNumber (int) – New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LayoutManagementBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.