HoleReportBuilderEnumQuadrantType Enumeration¶
NXOpen.Tooling.HoleReportBuilder.EnumQuadrantType is an alias for NXOpen.Tooling.HoleReportBuilderEnumQuadrantType
-
class
NXOpen.Tooling.
HoleReportBuilderEnumQuadrantType
¶ Bases:
object
Specifies the option of which quadrant is positive
Enum Members
Enum Member Enum Member Description PositiveQuadrantI First quadrant is positive PositiveQuadrantIi Second quadrant is positive PositiveQuadrantIii Third quadrant is positive PositiveQuadrantIv Forth quadrant is positive PositiveQuadrantAll All quadrant is positive -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-