HoleManufacturingNoteBuilderHoleIndexType Enumeration

NXOpen.Tooling.HoleManufacturingNoteBuilder.HoleIndexType is an alias for NXOpen.Tooling.HoleManufacturingNoteBuilderHoleIndexType

class NXOpen.Tooling.HoleManufacturingNoteBuilderHoleIndexType

Bases: object

the hole index type

Enum Members

Enum Member Enum Member Description
UserDefinedAndNumber
Alphabetic
Numeric
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.