HoleManufacturingNoteBuilderDefineByViewOrHoles Enumeration

NXOpen.Tooling.HoleManufacturingNoteBuilder.DefineByViewOrHoles is an alias for NXOpen.Tooling.HoleManufacturingNoteBuilderDefineByViewOrHoles

class NXOpen.Tooling.HoleManufacturingNoteBuilderDefineByViewOrHoles

Bases: object

the view selection or window selection type

Enum Members

Enum Member Enum Member Description
View
Holes
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.