ForceCalculationBuilderProcessTypes Enumeration¶
NXOpen.Tooling.ForceCalculationBuilder.ProcessTypes is an alias for NXOpen.Tooling.ForceCalculationBuilderProcessTypes
-
class
NXOpen.Tooling.
ForceCalculationBuilderProcessTypes
¶ Bases:
object
The process type.
Enum Members
Enum Member Enum Member Description Catalog catalog AngularBlanking angular blanking AngularEmbossing angular embossing AngularPiercing angular piercing Bending bending Blanking blanking Burring burring CircularDrawing circular drawing Counterboring counterboring Countersinking countersinking CylindricalIroning cylindrical ironing Flanging flanging Piercing piercing RoundEmbossing round embossing SquareDrawing square drawing UBending U bending VBending V bending VBendingTree V bending tree ZBending Z bending -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-