FastenerAssyHoleOperation Enumeration¶
NXOpen.Tooling.FastenerAssy.HoleOperation is an alias for NXOpen.Tooling.FastenerAssyHoleOperation
-
class
NXOpen.Tooling.
FastenerAssyHoleOperation
¶ Bases:
object
Represents the action on the hole menu of the fastener assembly.
Enum Members
Enum Member Enum Member Description Add Click the add hole group menu Remove Click the remove menu -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-