FaceSplitBuilderFaceSplitType Enumeration¶
NXOpen.Tooling.FaceSplitBuilder.FaceSplitType is an alias for NXOpen.Tooling.FaceSplitBuilderFaceSplitType
-
class
NXOpen.Tooling.
FaceSplitBuilderFaceSplitType
¶ Bases:
object
the type for Split Face
Enum Members
Enum Member Enum Member Description CurvesEdges using curve or edge for Split Face Plane using plane for Split Face Intersection using intersection curve of two body for Split Face Isocline using Isocline for Split Face -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-