ElectrodeCheckingBuilder Class¶
-
class
NXOpen.Tooling.
ElectrodeCheckingBuilder
¶ Bases:
NXOpen.Builder
Electrode Checking builder to check the touch status of all electrode.
To create a new instance of this class, use
NXOpen.Tooling.ElectrodeDesignCollection.CreateCheckingBuilder()
Default values.
Property Value InterSolid 1 MapFaceColor 1 SameParent 1 TouchArea 0 TouchBody 1 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
Electrode | Returns the electrode part to be checked with the workpiece part. |
ElectrodeNameFilter | Returns or sets the wildcard string to filter out the electrode part name. |
InterSolid | Returns or sets the option for generating the interference solid body. |
MapFaceColor | Returns or sets the option for mapping color of the touched face pair from workpiece to electrode. |
SameParent | Returns or sets the option for checking the workpiece and electrode part under the same part or not. |
SaveResultsInPart | Returns or sets the option for saving checking results in part. |
Tag | Returns the Tag for this object. |
TouchArea | Returns or sets the option for calculating the area of the touch sheet body. |
TouchBody | Returns or sets the option for generating the touch sheet body. |
Workpiece | Returns the workpiece part to be checked with the electrode part. |
WorkpieceNameFilter | Returns or sets the wildcard string to filter out the workpiece part name. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Electrode¶
-
ElectrodeCheckingBuilder.
Electrode
¶ Returns the electrode part to be checked with the workpiece part.
-------------------------------------
Getter Method
Signature
Electrode
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: None.
ElectrodeNameFilter¶
-
ElectrodeCheckingBuilder.
ElectrodeNameFilter
¶ Returns or sets the wildcard string to filter out the electrode part name.
-------------------------------------
Getter Method
Signature
ElectrodeNameFilter
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ElectrodeNameFilter
Parameters: electrodeNameFilter (str) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
InterSolid¶
-
ElectrodeCheckingBuilder.
InterSolid
¶ Returns or sets the option for generating the interference solid body.
-------------------------------------
Getter Method
Signature
InterSolid
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InterSolid
Parameters: interSolid (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
MapFaceColor¶
-
ElectrodeCheckingBuilder.
MapFaceColor
¶ Returns or sets the option for mapping color of the touched face pair from workpiece to electrode.
-------------------------------------
Getter Method
Signature
MapFaceColor
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MapFaceColor
Parameters: mapFaceColor (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
SameParent¶
-
ElectrodeCheckingBuilder.
SameParent
¶ Returns or sets the option for checking the workpiece and electrode part under the same part or not.
-------------------------------------
Getter Method
Signature
SameParent
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SameParent
Parameters: sameParent (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
SaveResultsInPart¶
-
ElectrodeCheckingBuilder.
SaveResultsInPart
¶ Returns or sets the option for saving checking results in part.
-------------------------------------
Getter Method
Signature
SaveResultsInPart
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SaveResultsInPart
Parameters: saveResultsInPart (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
TouchArea¶
-
ElectrodeCheckingBuilder.
TouchArea
¶ Returns or sets the option for calculating the area of the touch sheet body.
-------------------------------------
Getter Method
Signature
TouchArea
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TouchArea
Parameters: touchArea (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
TouchBody¶
-
ElectrodeCheckingBuilder.
TouchBody
¶ Returns or sets the option for generating the touch sheet body.
-------------------------------------
Getter Method
Signature
TouchBody
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TouchBody
Parameters: touchBody (bool) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Workpiece¶
-
ElectrodeCheckingBuilder.
Workpiece
¶ Returns the workpiece part to be checked with the electrode part.
-------------------------------------
Getter Method
Signature
Workpiece
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: None.
WorkpieceNameFilter¶
-
ElectrodeCheckingBuilder.
WorkpieceNameFilter
¶ Returns or sets the wildcard string to filter out the workpiece part name.
-------------------------------------
Getter Method
Signature
WorkpieceNameFilter
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WorkpieceNameFilter
Parameters: workpieceNameFilter (str) – New in version NX8.0.0.
License requirements: nx_electrode_wizard (“NX Electrode Wizard”)
Method Detail¶
Validate¶
-
ElectrodeCheckingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.