ElectrodeBlankBuilderBlankShape Enumeration¶
NXOpen.Tooling.ElectrodeBlankBuilder.BlankShape is an alias for NXOpen.Tooling.ElectrodeBlankBuilderBlankShape
-
class
NXOpen.Tooling.
ElectrodeBlankBuilderBlankShape
¶ Bases:
object
Represents the electrode blank shape option.
Enum Members
Enum Member Enum Member Description Block the shape of the blank is block Cylinder the shape of the blank is cylinder Undercut the shape of the blank is block to spark undercut area -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-