EdgePatchBuilderPatchStatus Enumeration¶
NXOpen.Tooling.EdgePatchBuilder.PatchStatus is an alias for NXOpen.Tooling.EdgePatchBuilderPatchStatus
-
class
NXOpen.Tooling.
EdgePatchBuilderPatchStatus
¶ Bases:
object
Settings of the patch status types.
Enum Members
Enum Member Enum Member Description NoLoopExisted No loop existed in list OneLoopExisted One loop existed in list MultiLoopsExisted More than one loops existed in list SomeLoopsExisted Some loops existed in list LoopNotPatched No loop is patched PatchedAndSomeSuppressed Some patched bodies are suppressed PatchedAndAllSuppressed All patched bodies are suppressed PatchedAndNoSuppressed No patched body is suppressed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-