DirectUnfoldBuilderBodyList Enumeration¶
NXOpen.Tooling.DirectUnfoldBuilder.BodyList is an alias for NXOpen.Tooling.DirectUnfoldBuilderBodyList
-
class
NXOpen.Tooling.
DirectUnfoldBuilderBodyList
¶ Bases:
object
The name list of bodies in current part. It is changed in selecting different part.
Enum Members
Enum Member Enum Member Description NotSet Default is none. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-