DirectUnfoldBuilderBend Enumeration¶
NXOpen.Tooling.DirectUnfoldBuilder.Bend is an alias for NXOpen.Tooling.DirectUnfoldBuilderBend
-
class
NXOpen.Tooling.
DirectUnfoldBuilderBend
¶ Bases:
object
The number of children bends in defining prebend.
Enum Members
Enum Member Enum Member Description Two two bends Three three bends Four four bends Five five bends Six six bends -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-