DieEngTrimAngleCheckBuilderDirectionOptions Enumeration

NXOpen.Tooling.DieEngTrimAngleCheckBuilder.DirectionOptions is an alias for NXOpen.Tooling.DieEngTrimAngleCheckBuilderDirectionOptions

class NXOpen.Tooling.DieEngTrimAngleCheckBuilderDirectionOptions

Bases: object

Options to determine the method to specify direction.

Enum Members

Enum Member Enum Member Description
ByVector
ByAngles
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.