DieDesignTrimPostBuilder Class¶
-
class
NXOpen.Tooling.
DieDesignTrimPostBuilder
¶ Bases:
NXOpen.Builder
Represents a Trim Post builder
To create a new instance of this class, use
NXOpen.Tooling.AutoDieCollection.CreateDieDesignTrimPostBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
BasePlane | Returns or sets the base plane used to create Trim Post |
BeltThickness | Returns or sets the belt thickness parameter of Trim Post section |
BoundaryCurves | Returns the boundary curves used to create Trim Post |
CAMRelief | Returns or sets the cam relief parameter of Trim Post section |
CamDirection | Returns or sets the cam direction used to create Trim Post |
MachineAllowance | Returns or sets the machine allowance used to rough offset product sheet |
Product | Returns the product selection |
Profiles | Returns the trim profiles used to create Trim Post |
ProfilesDirection | Returns or sets the trim profiles direction used to determine which side the Trim Post will be built, is true in the direction and false in the opposite direction |
Tag | Returns the Tag for this object. |
UseApproxSheetBody | Returns or sets the option to use the original sheet body or the rough offset sheet instead. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SeedPointInfo | Sets seed point information. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BasePlane¶
-
DieDesignTrimPostBuilder.
BasePlane
¶ Returns or sets the base plane used to create Trim Post
-------------------------------------
Getter Method
Signature
BasePlane
Returns: Return type: NXOpen.Plane
New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
BasePlane
Parameters: basePlane ( NXOpen.Plane
) –New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
BeltThickness¶
-
DieDesignTrimPostBuilder.
BeltThickness
¶ Returns or sets the belt thickness parameter of Trim Post section
-------------------------------------
Getter Method
Signature
BeltThickness
Returns: Return type: float New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
BeltThickness
Parameters: beltThickness (float) – New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
BoundaryCurves¶
-
DieDesignTrimPostBuilder.
BoundaryCurves
¶ Returns the boundary curves used to create Trim Post
-------------------------------------
Getter Method
Signature
BoundaryCurves
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
CAMRelief¶
-
DieDesignTrimPostBuilder.
CAMRelief
¶ Returns or sets the cam relief parameter of Trim Post section
-------------------------------------
Getter Method
Signature
CAMRelief
Returns: Return type: float New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
CAMRelief
Parameters: camRelief (float) – New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
CamDirection¶
-
DieDesignTrimPostBuilder.
CamDirection
¶ Returns or sets the cam direction used to create Trim Post
-------------------------------------
Getter Method
Signature
CamDirection
Returns: Return type: NXOpen.Direction
New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
CamDirection
Parameters: camDirection ( NXOpen.Direction
) –New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
MachineAllowance¶
-
DieDesignTrimPostBuilder.
MachineAllowance
¶ Returns or sets the machine allowance used to rough offset product sheet
-------------------------------------
Getter Method
Signature
MachineAllowance
Returns: Return type: float New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
MachineAllowance
Parameters: machineAllowance (float) – New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
Product¶
-
DieDesignTrimPostBuilder.
Product
¶ Returns the product selection
-------------------------------------
Getter Method
Signature
Product
Returns: Return type: NXOpen.SelectBody
New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
Profiles¶
-
DieDesignTrimPostBuilder.
Profiles
¶ Returns the trim profiles used to create Trim Post
-------------------------------------
Getter Method
Signature
Profiles
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
ProfilesDirection¶
-
DieDesignTrimPostBuilder.
ProfilesDirection
¶ Returns or sets the trim profiles direction used to determine which side the Trim Post will be built, is true in the direction and false in the opposite direction
-------------------------------------
Getter Method
Signature
ProfilesDirection
Returns: Return type: bool New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
ProfilesDirection
Parameters: profilesDirection (bool) – New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
UseApproxSheetBody¶
-
DieDesignTrimPostBuilder.
UseApproxSheetBody
¶ Returns or sets the option to use the original sheet body or the rough offset sheet instead.
The original sheet body is the user specified product body, which will be used to create the trim post features. When value is true, the original sheet body will be used, when value is false, the rough offset sheet will be used.
-------------------------------------
Getter Method
Signature
UseApproxSheetBody
Returns: Return type: bool New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
UseApproxSheetBody
Parameters: useExtractSheetBody (bool) – New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
SeedPointInfo¶
-
DieDesignTrimPostBuilder.
SeedPointInfo
¶ Sets seed point information.
Signature
SeedPointInfo(seedPoint, seedTangent)
Parameters: - seedPoint (list of float) –
- seedTangent (list of float) –
New in version NX9.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
DieDesignTrimPostBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.