DieDesignSettingBuilder Class¶
-
class
NXOpen.Tooling.
DieDesignSettingBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.DieDesignSettingBuilder
This class is for Die Design Setting UITo create a new instance of this class, use
NXOpen.Tooling.DieDesignSettingCollection.CreateDieDesignSettingBuilder()
Default values.
Property Value RoundoffInsertXYPosition 1 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
RoundoffInsertXYPosition | Returns or sets the option to roundoff insert X and Y position |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetParameters | Set the parameter number, names and values in the tree list into builder attribute. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
RoundoffInsertXYPosition¶
-
DieDesignSettingBuilder.
RoundoffInsertXYPosition
¶ Returns or sets the option to roundoff insert X and Y position
-------------------------------------
Getter Method
Signature
RoundoffInsertXYPosition
Returns: Return type: bool New in version NX12.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RoundoffInsertXYPosition
Parameters: roundoffInsertXYPosition (bool) – New in version NX12.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
SetParameters¶
-
DieDesignSettingBuilder.
SetParameters
¶ Set the parameter number, names and values in the tree list into builder attribute.
Signature
SetParameters(paraNames, paraValues)
Parameters: - paraNames (list of str) – an array of names
- paraValues (list of str) – an array of values
New in version NX7.5.0.
License requirements: None.
Validate¶
-
DieDesignSettingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.