DieDesPierceInsertBuilderDirection Enumeration

NXOpen.Tooling.DieDesPierceInsertBuilder.Direction is an alias for NXOpen.Tooling.DieDesPierceInsertBuilderDirection

class NXOpen.Tooling.DieDesPierceInsertBuilderDirection

Bases: object

Represents the thickness direction.

Enum Members

Enum Member Enum Member Description
Upper
Lower
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.