DieBaseBuilderPlatesNumberOpt Enumeration¶
NXOpen.Tooling.DieBaseBuilder.PlatesNumberOpt is an alias for NXOpen.Tooling.DieBaseBuilderPlatesNumberOpt
-
class
NXOpen.Tooling.
DieBaseBuilderPlatesNumberOpt
¶ Bases:
object
plates number options.
Enum Members
Enum Member Enum Member Description PlateFive plates number is 5 PlateEight plates number is 8 PlateNine plates number is 9 PlateTen plates number is 10 PlateTwelve plates number is 12 -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-