DieBaseBuilderDieBaseTypeOpt Enumeration¶
NXOpen.Tooling.DieBaseBuilder.DieBaseTypeOpt is an alias for NXOpen.Tooling.DieBaseBuilderDieBaseTypeOpt
-
class
NXOpen.Tooling.
DieBaseBuilderDieBaseTypeOpt
¶ Bases:
object
die bse types options.
Enum Members
Enum Member Enum Member Description Pdw progressive die type SingleDie single die type CompoundDie compound die type DrawDie draw die type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-