DefineNeutralFactorBuilderFormulaOptions Enumeration¶
NXOpen.Tooling.DefineNeutralFactorBuilder.FormulaOptions is an alias for NXOpen.Tooling.DefineNeutralFactorBuilderFormulaOptions
-
class
NXOpen.Tooling.
DefineNeutralFactorBuilderFormulaOptions
¶ Bases:
object
Specifies the formula used to calculate the neutral factor value
Enum Members
Enum Member Enum Member Description General General formula use the ratio of inner bend radius and thickness BendAllowance Bend allowance formula use different formula according to inner bend radius and thickness -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-