CopySolidBuilder Class¶
-
class
NXOpen.Tooling.
CopySolidBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.CopySolidBuilder
builder.To create a new instance of this class, use
NXOpen.Tooling.MoldwizardManager.CreateCopySolidBuilder()
Default values.
Property Value LinkToNewComponents 1 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CloneObject | Returns the clone client data. |
LinkToNewComponents | Returns or sets the link to new components |
MultipleComponents | Returns or sets the multiple components |
SelectBodies | Returns the solid bodies selected by user |
SelectParentPartOcc | Returns the parent part occurrence of the part which collects the copied solid bodies. |
Tag | Returns the Tag for this object. |
WizardType | Returns or sets the wizard type data. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CloneObject¶
-
CopySolidBuilder.
CloneObject
¶ Returns the clone client data.
-------------------------------------
Getter Method
Signature
CloneObject
Returns: A NXOpen.Tooling.CloneObject
instanceReturn type: NXOpen.Tooling.CloneObject
New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
LinkToNewComponents¶
-
CopySolidBuilder.
LinkToNewComponents
¶ Returns or sets the link to new components
-------------------------------------
Getter Method
Signature
LinkToNewComponents
Returns: Return type: bool New in version NX11.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
LinkToNewComponents
Parameters: linkToNewComponents (bool) – New in version NX11.0.1.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
MultipleComponents¶
-
CopySolidBuilder.
MultipleComponents
¶ Returns or sets the multiple components
-------------------------------------
Getter Method
Signature
MultipleComponents
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MultipleComponents
Parameters: multipleComponents (bool) – New in version NX11.0.0.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
SelectBodies¶
-
CopySolidBuilder.
SelectBodies
¶ Returns the solid bodies selected by user
-------------------------------------
Getter Method
Signature
SelectBodies
Returns: Return type: NXOpen.SelectBodyList
New in version NX11.0.0.
License requirements: None.
SelectParentPartOcc¶
-
CopySolidBuilder.
SelectParentPartOcc
¶ Returns the parent part occurrence of the part which collects the copied solid bodies.
-------------------------------------
Getter Method
Signature
SelectParentPartOcc
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX11.0.0.
License requirements: None.
WizardType¶
-
CopySolidBuilder.
WizardType
¶ Returns or sets the wizard type data.
-------------------------------------
Getter Method
Signature
WizardType
Returns: Return type: NXOpen.Tooling.ToolingApplication
New in version NX11.0.2.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
-------------------------------------
Setter Method
Signature
WizardType
Parameters: wizardType ( NXOpen.Tooling.ToolingApplication
) –New in version NX11.0.2.
License requirements: ug_mold_design (“UG MOLD”) OR prog_die_wizard (“UG/Progressive Die Wizard”)
Method Detail¶
Validate¶
-
CopySolidBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.