CoolingDefineChannelBuilderExtensionTypes Enumeration

NXOpen.Tooling.CoolingDefineChannelBuilder.ExtensionTypes is an alias for NXOpen.Tooling.CoolingDefineChannelBuilderExtensionTypes

class NXOpen.Tooling.CoolingDefineChannelBuilderExtensionTypes

Bases: object

The extension types of channel

Enum Members

Enum Member Enum Member Description
NoExtension No extension
AlongExtrusionDirection Extend channel to boundary body along the extrusion direction
AlongReverseExtrusionDirection Extend channel to boundary body along the reverse extrusion direction
AlongBothDirections Extend channel to boundary body along both direction
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.