CoolingConnectBuilder Class¶
-
class
NXOpen.Tooling.
CoolingConnectBuilder
¶ Bases:
NXOpen.Builder
The builder class for Cooling connection which assists you to create channel and connect it to other channels.
To create a new instance of this class, use
NXOpen.Tooling.CoolingConnectCollection.CreateCoolingConnectBuilder()
Default values.
Property Value DefineConnectVector 0 DefineStartPoint 0 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
ConnectVector | Returns or sets the vector specified for creating connecting channel. |
DefineConnectVector | Returns or sets the value which specifies whether to define the vector of the connect channel or not. |
DefineStartPoint | Returns or sets the value which specifies whether to define the start point or not. |
FirstChannel | Returns the first channel to be connected. |
SecondChannel | Returns the second channel to be connected. |
StartPoint | Returns or sets the point for changing the start position of the connecting channel. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ConnectVector¶
-
CoolingConnectBuilder.
ConnectVector
¶ Returns or sets the vector specified for creating connecting channel.
-------------------------------------
Getter Method
Signature
ConnectVector
Returns: Return type: NXOpen.Direction
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConnectVector
Parameters: connectVector ( NXOpen.Direction
) –New in version NX7.5.0.
License requirements: None.
DefineConnectVector¶
-
CoolingConnectBuilder.
DefineConnectVector
¶ Returns or sets the value which specifies whether to define the vector of the connect channel or not.
-------------------------------------
Getter Method
Signature
DefineConnectVector
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefineConnectVector
Parameters: defineConnectVector (bool) – New in version NX7.5.0.
License requirements: None.
DefineStartPoint¶
-
CoolingConnectBuilder.
DefineStartPoint
¶ Returns or sets the value which specifies whether to define the start point or not.
-------------------------------------
Getter Method
Signature
DefineStartPoint
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DefineStartPoint
Parameters: defineStartPoint (bool) – New in version NX7.5.0.
License requirements: None.
FirstChannel¶
-
CoolingConnectBuilder.
FirstChannel
¶ Returns the first channel to be connected.
-------------------------------------
Getter Method
Signature
FirstChannel
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
SecondChannel¶
-
CoolingConnectBuilder.
SecondChannel
¶ Returns the second channel to be connected.
-------------------------------------
Getter Method
Signature
SecondChannel
Returns: Return type: NXOpen.SelectBody
New in version NX7.5.0.
License requirements: None.
StartPoint¶
-
CoolingConnectBuilder.
StartPoint
¶ Returns or sets the point for changing the start position of the connecting channel.
-------------------------------------
Getter Method
Signature
StartPoint
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPoint
Parameters: startPoint ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
CoolingConnectBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.