ConcurrentDesignManagementBuilder Class¶
-
class
NXOpen.Tooling.
ConcurrentDesignManagementBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.ConcurrentDesignManagementBuilder
to support concurrent design workflow management.To create a new instance of this class, use
NXOpen.Tooling.WorkflowManagementCollection.CreateConcurrentDesignManagementBuilder()
Default values.
Property Value SetAsMyDefaultTask 0 UpdateOptions SaveMyComponents New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
DesignTasks | Returns or sets the designer names. |
DesignerName | Returns or sets the designer name. |
ProjectLeader | Returns or sets the project leader name. |
SelectComponent | Returns the selected component to assign to a designer. |
SelectedDesignerIndex | Returns or sets the index of the selected designer. |
SetAsMyDefaultTask | Returns or sets the option to set as the current user’s default task. |
Tag | Returns the Tag for this object. |
TaskDescription | Returns or sets the task description string |
Type | Returns or sets the type of concurrent design management. |
UpdateOptions | Returns or sets the update type. |
UserName | Returns or sets the user name to login. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ConcurrentDesignManagementBuilderTypes Enumeration | Specifies the types of concurrent design management. |
ConcurrentDesignManagementBuilderUpdateTypes Enumeration | Specifies the types of the update action. |
Property Detail¶
DesignTasks¶
-
ConcurrentDesignManagementBuilder.
DesignTasks
¶ Returns or sets the designer names.
-------------------------------------
Getter Method
Signature
DesignTasks
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignTasks
Parameters: designTasks (str) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
DesignerName¶
-
ConcurrentDesignManagementBuilder.
DesignerName
¶ Returns or sets the designer name.
-------------------------------------
Getter Method
Signature
DesignerName
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignerName
Parameters: designerName (str) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
ProjectLeader¶
-
ConcurrentDesignManagementBuilder.
ProjectLeader
¶ Returns or sets the project leader name.
-------------------------------------
Getter Method
Signature
ProjectLeader
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ProjectLeader
Parameters: projectLeader (str) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
SelectComponent¶
-
ConcurrentDesignManagementBuilder.
SelectComponent
¶ Returns the selected component to assign to a designer.
-------------------------------------
Getter Method
Signature
SelectComponent
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: None.
SelectedDesignerIndex¶
-
ConcurrentDesignManagementBuilder.
SelectedDesignerIndex
¶ Returns or sets the index of the selected designer.
-------------------------------------
Getter Method
Signature
SelectedDesignerIndex
Returns: Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedDesignerIndex
Parameters: selectedDesignerIndex (int) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
SetAsMyDefaultTask¶
-
ConcurrentDesignManagementBuilder.
SetAsMyDefaultTask
¶ Returns or sets the option to set as the current user’s default task.
-------------------------------------
Getter Method
Signature
SetAsMyDefaultTask
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SetAsMyDefaultTask
Parameters: setAsMyDefaultTask (bool) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
TaskDescription¶
-
ConcurrentDesignManagementBuilder.
TaskDescription
¶ Returns or sets the task description string
-------------------------------------
Getter Method
Signature
TaskDescription
Returns: Return type: str New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TaskDescription
Parameters: taskDescription (str) – New in version NX10.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
Type¶
-
ConcurrentDesignManagementBuilder.
Type
¶ Returns or sets the type of concurrent design management.
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Tooling.ConcurrentDesignManagementBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Tooling.ConcurrentDesignManagementBuilderTypes
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
UpdateOptions¶
-
ConcurrentDesignManagementBuilder.
UpdateOptions
¶ Returns or sets the update type.
-------------------------------------
Getter Method
Signature
UpdateOptions
Returns: Return type: NXOpen.Tooling.ConcurrentDesignManagementBuilderUpdateTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpdateOptions
Parameters: updateOptions ( NXOpen.Tooling.ConcurrentDesignManagementBuilderUpdateTypes
) –New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
UserName¶
-
ConcurrentDesignManagementBuilder.
UserName
¶ Returns or sets the user name to login.
-------------------------------------
Getter Method
Signature
UserName
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UserName
Parameters: userName (str) – New in version NX8.0.0.
License requirements: prog_die_wizard (“UG/Progressive Die Wizard”) OR nx_engineering_die_wizard (“NX Engineering Die Wizard”)
Method Detail¶
Validate¶
-
ConcurrentDesignManagementBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.