ClearanceManagementBuilderType Enumeration

NXOpen.Tooling.ClearanceManagementBuilder.Type is an alias for NXOpen.Tooling.ClearanceManagementBuilderType

class NXOpen.Tooling.ClearanceManagementBuilderType

Bases: object

Specifies type to assign or check clearances

Enum Members

Enum Member Enum Member Description
AssignClearances
CheckClearances
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.