ChangeoverManagementBuilder Class¶
-
class
NXOpen.Tooling.
ChangeoverManagementBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Tooling.ChangeoverManagementBuilder
to support changeover workflow management.To create a new instance of this class, use
NXOpen.Tooling.WorkflowManagementCollection.CreateChangeoverManagementBuilder()
Default values.
Property Value AddComponentsExclusively 0 RenameComponent 0 New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AddComponentsExclusively | Returns or sets the exclusive adding |
ChangeoverName | Returns or sets the name of the to-be-created changeover. |
ClonedProductName | Returns or sets the name of the cloned product pack used to create a new changeover. |
NewChangeoverName | Returns or sets the new name of the selected changeover. |
RenameComponent | Returns or sets the option to rename the components of the to-be-created changeover. |
SelectComponents | Returns the selection of components to be added to or removed from a changeover. |
SelectProduct | Returns the selection of product for which to create changeover. |
SelectedArrangementName | Returns or sets the name of the selected changeover arrangement. |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type of changeover management. |
Methods¶
Method | Description |
---|---|
AddToChangeover | Add selected components to the selected changeover. |
Commit | Commits any edits that have been applied to the builder. |
DeleteArrangement | Delete the selected changeover. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
RemoveFromChangeover | Remove selected components from the selected changeover. |
RenameArrangement | Rename the selected changeover. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UseArrangement | Set the selected changeover as current used one. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ChangeoverManagementBuilderTypes Enumeration | Specifies the types of changeover management. |
Property Detail¶
AddComponentsExclusively¶
-
ChangeoverManagementBuilder.
AddComponentsExclusively
¶ Returns or sets the exclusive adding
-------------------------------------
Getter Method
Signature
AddComponentsExclusively
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddComponentsExclusively
Parameters: addComponentsExclusively (bool) – New in version NX8.0.0.
License requirements: None.
ChangeoverName¶
-
ChangeoverManagementBuilder.
ChangeoverName
¶ Returns or sets the name of the to-be-created changeover.
-------------------------------------
Getter Method
Signature
ChangeoverName
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChangeoverName
Parameters: changeoverName (str) – New in version NX8.0.0.
License requirements: None.
ClonedProductName¶
-
ChangeoverManagementBuilder.
ClonedProductName
¶ Returns or sets the name of the cloned product pack used to create a new changeover.
-------------------------------------
Getter Method
Signature
ClonedProductName
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClonedProductName
Parameters: clonedProductName (str) – New in version NX8.0.0.
License requirements: None.
NewChangeoverName¶
-
ChangeoverManagementBuilder.
NewChangeoverName
¶ Returns or sets the new name of the selected changeover.
-------------------------------------
Getter Method
Signature
NewChangeoverName
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NewChangeoverName
Parameters: newChangeoverName (str) – New in version NX8.0.0.
License requirements: None.
RenameComponent¶
-
ChangeoverManagementBuilder.
RenameComponent
¶ Returns or sets the option to rename the components of the to-be-created changeover.
-------------------------------------
Getter Method
Signature
RenameComponent
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RenameComponent
Parameters: renameComponent (bool) – New in version NX8.0.0.
License requirements: None.
SelectComponents¶
-
ChangeoverManagementBuilder.
SelectComponents
¶ Returns the selection of components to be added to or removed from a changeover.
-------------------------------------
Getter Method
Signature
SelectComponents
Returns: Return type: NXOpen.Assemblies.SelectComponentList
New in version NX8.0.0.
License requirements: None.
SelectProduct¶
-
ChangeoverManagementBuilder.
SelectProduct
¶ Returns the selection of product for which to create changeover.
-------------------------------------
Getter Method
Signature
SelectProduct
Returns: Return type: NXOpen.Assemblies.SelectComponent
New in version NX8.0.0.
License requirements: None.
SelectedArrangementName¶
-
ChangeoverManagementBuilder.
SelectedArrangementName
¶ Returns or sets the name of the selected changeover arrangement.
-------------------------------------
Getter Method
Signature
SelectedArrangementName
Returns: Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedArrangementName
Parameters: arrangementName (str) – New in version NX8.0.0.
License requirements: None.
Type¶
-
ChangeoverManagementBuilder.
Type
¶ Returns or sets the type of changeover management.
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Tooling.ChangeoverManagementBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Tooling.ChangeoverManagementBuilderTypes
) –New in version NX8.0.0.
License requirements: None.
Method Detail¶
AddToChangeover¶
-
ChangeoverManagementBuilder.
AddToChangeover
¶ Add selected components to the selected changeover.
Signature
AddToChangeover()
New in version NX8.0.0.
License requirements: None.
DeleteArrangement¶
-
ChangeoverManagementBuilder.
DeleteArrangement
¶ Delete the selected changeover.
Signature
DeleteArrangement(removeComponents)
Parameters: removeComponents (bool) – New in version NX8.0.0.
License requirements: None.
RemoveFromChangeover¶
-
ChangeoverManagementBuilder.
RemoveFromChangeover
¶ Remove selected components from the selected changeover.
Signature
RemoveFromChangeover()
New in version NX8.0.0.
License requirements: None.
RenameArrangement¶
-
ChangeoverManagementBuilder.
RenameArrangement
¶ Rename the selected changeover.
Signature
RenameArrangement()
New in version NX8.0.0.
License requirements: None.
UseArrangement¶
-
ChangeoverManagementBuilder.
UseArrangement
¶ Set the selected changeover as current used one.
Signature
UseArrangement()
New in version NX8.0.0.
License requirements: None.
Validate¶
-
ChangeoverManagementBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.