CalculateAreaBuilderSheetMethodType Enumeration¶
NXOpen.Tooling.CalculateAreaBuilder.SheetMethodType is an alias for NXOpen.Tooling.CalculateAreaBuilderSheetMethodType
-
class
NXOpen.Tooling.
CalculateAreaBuilderSheetMethodType
¶ Bases:
object
Represents the methods to create the projected sheet body.
Enum Members
Enum Member Enum Member Description Curve Using projected curve method to create the sheet body. Mesh Using mesh method to create the sheet body. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-